Pompa Ansiklopedisi (İngilizce)

51 sonuçlardan 41 dan 50 e kadar gösteriyor
Convector
A convector is a heating surface that transfers heat mainly by convection. Convection is the process by which heat is transferred when cooler air flows over the warm surface of a solid material.
Cooling ceiling
Water-carrying cooling ceilings can be used as a supplement, if cooled-air temperature regulation systems are insufficient. The cooling effect is primarily achieved through the absorption of heat, with convection being a secondary function.
Cooling jacket
A cooling jacket enables a portion of the pumped liquid or an external liquid to be circulated around the motor stator housing. This absorbs excess heat by forced convection, ensuring efficient cooling of the pump.
Cooling surface
A cooling surface is used for cooling of outside air before injection into the building. A cooling surface can be an integrated part of an AHU or placed directly in an air injection duct.
Cooling tower
A cooling tower is used to remove excess heat from an air-conditioning system if the heat cannot be utilised for another purpose.
COP (Coefficient of performance)
Coefficient of performance (COP), is an expression of the efficiency of a heat pump. When calculating the COP for a heat pump, the heat output from the condenser (Q) is compared to the power supplied to the compressor (W).
Corrosion
Corrosion can occur on external and internal surfaces of pipes, tanks and radiators. In the design phase various issues have to be considered such as pipe material, insulation, medium, humidity and air purging etc.
Corrosion fatigue
Corrosion fatigue describes a situation where a metal is exposed to both mechanical fatigue and corrosion simultaneously.
COSP (Coefficient of system performance)
The COSP of a heat pump is based on the total heat extracted (also referred to as Q) in relation to the energy supplied to the heat pump (also referred to as W).
Crevice corrosion
Crevice corrosion is a localized form of corrosion attack.